Pipe Network Concept

To introduce the Pipe Network concept, we can use a mechanical analogy.

In this figure, the mechanical system is composed of three-axes and driven by one motor.

  • All axes are connected to the motor through shafts, gears and cams.
  • When the motor is in motion, all axes are moving synchronously.
  • The speed relation between the Master and the Axis is achieved by using a mechanical Gear.
  • A mechanical cam is used to get linear motion from a rotating wheel.

Figure 5-6: Mechanical System

The Pipe Network in this figure corresponds to the mechanical system described above.
The pipe concept is a one-to-one translation of a mechanical system into the logical world.

Pipe Network Structure

Figure 5-7: Pipe Network Structure

In our Pipe Network, the analogy is:

  • The main motor of the mechanical machine becomes a Virtual Master Pipe Block.
  • The gear boxes becomes Gear Blocks.
  • The mechanical cam becomes a Cam Block.
  • The axes becomes Axis Blocks.

The Pipe Network concept allows motion engineers to define, in a very natural way, the physical relationships between the different axes of their machine.

This modular approach provides a solution for almost any multi-axis requirements. It remains open for new, additional functions that can be required in the future.

Concept Link IconSee Also